Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnCollectorChanged Method
The type of collector change.
The list of impacted collectors.


OnCollectorChanged Method
Invoked by the remote server to transmit collector subscription details.
Syntax
Public Sub OnCollectorChanged( _
   ByVal changetype As ChangeType, _
   ByVal collectors As System.Collections.Generic.List(Of Collector) _
) 

Parameters

changetype
The type of collector change.
collectors
The list of impacted collectors.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also