Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnOpening Method
Event source.
Event data.


OnOpening Method
Invoked when the connection object completes transition from the opening to opened states.
Syntax
Protected Sub OnOpening( _
   ByVal sender As System.Object, _
   ByVal e As System.EventArgs _
) 

Parameters

sender
Event source.
e
Event data.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also