Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / PublishGetDestinationServerEvent Event


PublishGetDestinationServerEvent Event (ServerConnection)
Occurs when a collector responds with the destination server name.
Syntax
Public Event PublishGetDestinationServerEvent As PublishGetDestinationServerHandler
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also