Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnOpened Method
Event source.
Event data.


OnOpened Method
Invoked when the connection object first enters the opening states.
Syntax
Protected Sub OnOpened( _
   ByVal sender As System.Object, _
   ByVal e As System.EventArgs _
) 

Parameters

sender
Event source.
e
Event data.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also