Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnCollectorCurrentValueResponse Method
Whether this is the final response.
Overall operation status.
The set of current tag values.
List of tags with errors.


OnCollectorCurrentValueResponse Method
Invoked by the remote server to transmit current collector tag values. Requesting many current values may generate multiple individual responses.
Syntax
Public Sub OnCollectorCurrentValueResponse( _
   ByVal final As System.Boolean, _
   ByVal status As Status, _
   ByVal dataset As DataSet, _
   ByVal errors As ItemErrors _
) 

Parameters

final
Whether this is the final response.
status
Overall operation status.
dataset
The set of current tag values.
errors
List of tags with errors.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also