Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnMessageAdded Method
A newly generated message.


OnMessageAdded Method
Invoked by the remote server to transmit message subscription details.
Syntax
Public Sub OnMessageAdded( _
   ByVal message As Message _
) 

Parameters

message
A newly generated message.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also