Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnPublishGetDestinationServer Method
Indication of how the request was processed.
Destination Historian server name.


OnPublishGetDestinationServer Method
Invoked by the remote server to transmit the requested destination server name.
Syntax
Public Sub OnPublishGetDestinationServer( _
   ByVal status As Status, _
   ByVal destinationServer As System.String _
) 

Parameters

status
Indication of how the request was processed.
destinationServer
Destination Historian server name.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also