Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ServerConnection Class / OnCollectorControlResponse Method
Indication of how the request was processed.


OnCollectorControlResponse Method
Invoked by the remote server to transmit the result of a control request.
Syntax
Public Sub OnCollectorControlResponse( _
   ByVal status As Status _
) 

Parameters

status
Indication of how the request was processed.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also