GE Vernova began shipping the Mark* VIe in 2004 and it’s used today on all of our latest heavy-duty and aeroderivative gas turbines. That is more than two decades of continuous production and active investment.
Today, more than 7,000 Mark VIe systems are installed on gas turbines, and around 800 to 900 of them in the aeroderivative fleet. Built for extended life, the Mark VIe is used in the installed base that generates approximately 25% of the world's electricity, demonstrating itself as a proven control system in the field.
The Mark V and Mark VI shared a fundamental architectural constraint. I/O modules sat inside a rack, and often multiple layers of circuit boards as the backplane, that could not be repaired. As each platform aged and a next-generation system arrived, the installed population of the previous one shrank. Supporting that rack became the first thing that determined end-of-life. Every generation of controls before the Mark VIe followed this pattern, including third-party PLCs and comparable platforms. The Mark VIe removed the rack and improved the lifecycle considerably.

The Mark VIe is built around distinct, independently serviceable building blocks that include the software, the main CPU, a communications switch, and the I/O packs that handle field I/O. Each hardware building block requires 28-volt DC power and Ethernet communications. Notably absent are a rack, rack power supplies, and a distinct form factor.
That shared component hardware interface standard of lower voltage power and an Ethernet connection is one of the reasons for the platform's longevity. The envelope each component is in can evolve indefinitely, provided the next-generation revision maintains those two interface requirements. The latest CPU or revised I/O pack drops into an existing system without requiring the operator to change anything else.
When a component reaches obsolescence, the sustaining engineering team configures a replacement, whether to address parts availability or a field reliability issue, and releases a different version; the operator replaces that component only. A unit that has been running the same I/O pack for 15 years can be updated without a hardware platform migration. One of the platform's most significant operational advantages is that once you replace the component and upgrade the software, the system is back in service.

Common modular upgrades include CPU upgrades (to support features like Model-Based Control), HMI and I/O pack replacements, and new power supply and network hardware.
GE Vernova formally manages Mark VIe hardware components through three defined phases, documented in the Mark VIe Control System Extended Lifecycle Policy.
This three-phase model gives operators something previous control system generations could not: a predictable, documented planning horizon, with specific action recommendations at each stage.

Since 2004, the Mark VIe platform has gone through multiple generations of processor technology, multiple I/O pack data acquisition upgrades, and significant evolution in communication protocols, smart device integration, and cybersecurity architecture. The industry 20 years ago and the industry today are two different places. What has not changed is the fundamental software suite delivering those advances.
GE Vernova manages Mark VIe software in two states:
Aeroderivative fleets are under growing pressure on cybersecurity. Faster start requirements, higher cycling rates, greater use of providing black start capable generation, and tightening OT security standards have placed demands on owners that historically operated under lighter requirements. A cybersecurity plan and supporting technology is no longer optional.
The Mark VIe addresses this through a defense-in-depth approach across all components. OTArmor* provides hardened network architecture, active monitoring, data loss protection, centralized backup/restore capability, and patch management. Coupled with a Controls Lifecare Services Multi-Year Agreement (CLS MYA), customers can benefit from representative hardware environment tested software updates and security patching on a continuous basis.
Cybersecurity is built into the platform from the start and maintained through lifecycle offerings supporting a site’s compliance program.
CLS helps operators execute against the hardware and software lifecycle models. Available as a multi-year agreement, CLS covers hardware components, ControlST* software updates, network switch firmware, security patching, and lifecycle assessments through a dashboard that tracks the specific hardware and software status of the installed system. It also supports long-term budget planning for incremental upgrades and parts inventory.
This communication contains forward-looking statements. Actual results may differ materially from those projected due to risks and uncertainties. GE Vernova undertakes no obligation to update these statements.

Robert White
Sr. Sales Manager, Control Solutions and Services, GE Vernova
Rob has focused on the controls retrofit space for over 25 years, supporting applications within steam, industrial gas, aero gas, plant, hydro, and generator environments. Early in his career, he was shadowing a field engineer who stated, “I know less now than when I began, because I now realize how much more there is to know." This has stayed with him as he pursues continuous learning in his field. Based out of upstate New York, he enjoys boating on the freshwater lakes, hiking, spending time with his family, and playing soccer.
Contact us
*Trademark of GE Vernova and/or its affiliates