Prefer to listen?

Stream our audio version

00:00:00 / 00:00:00

Vietnam is entering a defining period in its energy transition.

 
Rapid industrial growth, urban expansion, rising electricity demand, and increasing integration of renewables are placing new demands on the country’s power system. To support long-term economic development, Vietnam requires generation solutions that can be deployed quickly, have operational flexibility, and maintain grid reliability under high renewable energy penetration.

Vietnam’s energy system is evolving rapidly

Vietnam’s economy continues to expand across manufacturing, infrastructure, commercial operations, and residential development. At the same time, the country is accelerating renewable energy deployment and modernizing its power infrastructure to support future growth.

These changes are creating several interconnected challenges for grid operators and power developers:

  • Electricity needs continue to rise across industrial and urban centers
  • Renewable integration increases operational variability across the grid
  • New generation capacity must be added faster to maintain reliability
  • Grid operators require dispatchable resources that can respond quickly during changing demand conditions

Traditional power infrastructure projects often require extended construction timelines. In fast-growing economies, however, delayed capacity additions may affect industrial productivity, infrastructure planning, and overall energy security.

Why flexibility matters as renewable capacity grows

Wind and solar are becoming a larger part of Vietnam’s energy mix. While renewable generation supports long-term transition objectives, intermittent generation also increases the need for flexible resources that can stabilize the grid during fluctuations in renewable output or rapid changes in demand.

Fast-start aeroderivative gas turbines are well-suited for this role because they can:
 

areo-unit-benefits-to-fast-start.jpg

 
As renewable penetration increases, operational flexibility becomes increasingly important for maintaining system stability and supporting economic continuity.

A practical approach to fast-response generation

To help address these evolving requirements, GE Vernova offers aeroderivative gas power solutions engineered for rapid deployment and operational flexibility.

The LM6000VELOX* gas turbine solution is based on GE Vernova’s LM6000* aeroderivative gas turbine technology and uses a modular, pre-engineered configuration intended to simplify site execution and reduce installation timelines.

For Vietnam, this approach aligns closely with the need for fast deployable generation capacity while supporting a more dynamic power system.

Why the LM6000VELOX package is relevant for Vietnam

Fast deployment

The LM6000VELOX package uses a factory-assembled, modularized configuration that can help reduce on-site construction complexity and accelerate commissioning activities compared with conventional plant configurations.

For regions facing near-term supply-and-demand pressure, shorter installation timelines can help bring generation capacity online more quickly and support the expansion of industrial and urban load centers.

Operational flexibility

Aeroderivative gas turbines are engineered for fast starts, rapid ramping capability, and flexible operation across changing grid conditions.

These characteristics can help support renewable integration by providing dispatchable generation when wind or solar output fluctuates. For Vietnam, operational flexibility can support broader grid modernization efforts while helping maintain reliability during periods of variability.

Reliable grid support

Reliable electricity remains essential for manufacturing competitiveness, infrastructure expansion, and energy security. The LM6000 platform has been deployed across demanding operating environments and can provide rapid response support during peak demand periods, seasonal fluctuations, or unexpected grid events.

Scalable application support

The LM6000VELOX gas turbine can support multiple applications, including:

  • Peaking power generation
  • Utility and industrial power generation
  • Grid stability support
  • Fast-track capacity additions
  • Regional grid reinforcement

This flexibility allows the solution to support varying infrastructure requirements and operating conditions across Vietnam.

Experience with fast-track gas power deployment

GE Vernova recently deployed the LM6000VELOX gas turbine solution at a major aeroderivative power plant project in Tennessee, US. The customer installed 10 units totaling approximately 550 MW of capacity, demonstrating how aeroderivative technology can help meet large-scale power demand while maintaining deployment flexibility. The project also highlights how modular gas power infrastructure can help customers add dispatchable generation capacity with reduced site complexity and faster deployment timelines, cutting installation and commissioning schedules by roughly 40%.

While every power system has unique operational requirements, the broader challenge remains consistent across many regions: bringing reliable generation online quickly while supporting a more flexible grid.

That challenge is becoming increasingly relevant in Vietnam as electricity demand rises and renewable penetration expands. As the country plans for significant additions of flexible generation capacity, projects such as this demonstrate how aeroderivative solutions can help meet large-scale system demand while providing the operational flexibility needed to complement renewables.

Supporting Vietnam’s long-term energy transition

Vietnam’s long-term energy future will likely require a balanced generation portfolio that combines renewable growth with technologies that support reliability and operational flexibility.

Aeroderivative gas turbine solutions can support this transition by:

  • Providing fast-response generation during peak demand periods
  • Supporting grid stability alongside renewable generation by providing a variety of grid ancillary services
  • Accelerating access to additional generation capacity
  • Strengthening overall energy security and system resilience
f2.png

As Vietnam continues modernizing its energy infrastructure, fast-response gas power solutions can help address near-term reliability needs while supporting longer-term power system transition objectives.

Building a more resilient power system

Vietnam’s power sector is evolving quickly. Rising electricity demand, renewable integration, and grid modernization are increasing the need for generation solutions that combine speed, flexibility, and reliability.

GE Vernova’s LM6000VELOX gas turbine solution is engineered to help address these challenges through faster deployment timelines, operational agility, and dependable power generation. As Vietnam continues strengthening its energy infrastructure, flexible gas power can support grid resilience, renewable integration, and long-term energy security.

image-12.png

Shanshan Liang

Product Champion, Aeroderivative Gas Turbines
GE Vernova

As Product Champion for Aeroderivative Gas Turbines (China & Asia) at GE Vernova's Gas Power business, Shanshan Liang supports the positioning, promotion, and development of comprehensive solutions for aeroderivative gas turbine products across the region. She proactively collaborates with customers, EPCs, and partners during early project stages to define requirements, identify applicable technologies, and tailor holistic solutions. She also oversees regional market analysis, business development, and the formulation and execution of decarbonization and energy transition strategies.

Contact us

Speak with an expert today to learn more

*Trademark of GE Vernova and/or its affiliates.