Overview

The Nhon Trach 3 & 4 project demonstrates how high-efficiency combined-cycle gas technology can help support grid stability and emissions reduction as Vietnam expands LNG infrastructure.

The challenge

Vietnam’s power sector faced rising electricity demand, growing renewable penetration, and a need to reduce reliance on coal while maintaining system reliability. PV Power needed a large-scale facility with fast start-up, load flexibility, and proximity to demand centers.

The solution

GE Vernova provided two blocks that each included:

  • A 9HA.02 gas turbine
  • A STF-D650 steam turbine
  • A W88 generator
  • A Once-Through Heat Recovery Steam Generator (OT HRSG)
  • A Mark* VIe Distributed Control System

Each block (unit) can produce more than 800 megawatts. The scope also included long-term collaboration frameworks to support operations and potential efficiency improvements at existing PV Power assets.

Outcomes

Combined-cycle capacity and emissions performance

With both units in commercial operation, the plant delivers large-scale, flexible power and supports lower lifecycle emissions than coal-fired generation. The plant’s configuration also includes a Mark VIe distributed control system, supporting precise operational management and monitoring. Near Vietnam’s southern load center, the site enables efficient connection to the regional grid to enhance national energy security. The project also creates a framework for future HA-class combined-cycle installations in the country, providing a reference for system integration, maintenance, and long-term operational planning.

"

This first-of-its-kind project is expected to open a new chapter for gas power generation in Vietnam. We are proud to support the country’s energy goals through the development of its first HA-class power plant

Ramesh Singaram

President and CEO, Asia, GE Vernova Gas Power business

Contact Us 

Want to find out more about the 9HA gas turbine?