Exhaust gas recirculation for post-combustion carbon capture
Unlock greater cost savings with GE Vernova’s Exhaust Gas Recirculation (EGR) solution—a technique to make post-combustion carbon capture more efficient.
Adding value
Gas power plants, especially combined cycle power plants, are expected to play a key role in the energy transition due to their flexibility in meeting changing grid demands. The CO2 in the exhaust from these plants can be reduced by 95% or more using post-combustion carbon capture systems (CCS).
However, capturing CO2 can be costly, remaining a main challenge. Therefore, GE Vernova is working to improve the economics of carbon capture with techniques that include EGR. By cooling and cleaning 30–40% of the plant’s exhaust and feeding it back into the gas turbine—leaving the remaining 60–70% for the CCS island—EGR significantly reduces the physical size and energy demand of the capture system. The result? This reduces the size and energy demand of the CCS, making it more cost-effective and efficient path to lower emissions.
By working with multiple carbon capture providers around the globe, GE Vernova has confirmed through studies the benefits to the carbon capture system when EGR is part of an integrated natural gas combined cycle (NGCC) and CCS facility. In addition to benefiting the carbon capture system, the EGR system also benefits the combined cycle power plant.
GE Vernova is currently the only provider offering EGR for carbon capture, which can be deployed at both new and existing combined-cycle power plants.
Learn how integrating EGR into a combined cycle power plant with carbon capture can help improve overall system performance and efficiency.
Processing a split of the exhaust flow with a higher CO2 concentration means a smaller, less expensive carbon capture system.
Higher CO2 concentration in the exhaust flow means less energy required to separate CO2 from solvent, leaving more power for the grid.
Lower levels of oxygen in the exhaust flow reduces oxidation of the solvent, reducing the cost of replacement solvent.
Higher CO2 concentration in the exhaust flow can improve overall CO2 capture efficiency.
Reduced inlet bleed heat (IBH) results in improved part load efficiency.
At GE Vernova, our studies predict lower NOx, particulate matter, and CO emissions.
Understanding the flow
Instead of sending all exhaust from a combined cycle gas turbine directly to a carbon capture plant, GE Vernova’s EGR solution recirculates a portion of that exhaust back into the gas turbine inlet.
The result? A higher-concentration CO2 in the stream goes to the carbon capture equipment and less total exhaust must be processed, reducing both capture energy requirements and system size.
Our experience
At GE Vernova, we began studying EGR in 2006 for NOx reduction. More recently, we confirmed the benefits of using EGR in a NGCC with post-combustion carbon capture through laboratory testing and two FEED studies: Southern Company’s Plant Barry and NZT Power.
Webinar
Discover how EGR and integrated design strategies are helping move CCS from concept to deployment—supported by real-world lessons from NZT Power.
Matt Davidsaver
CCS Product Champion/GE Vernova
Laurent Thomas
Licensing Technology Manager- CO2 Capture Technologies/Shell Catalysts & Technologies
Ben Apperly
Business Development Manager- Decarbonization/Technip Energies
Resources
Want to dive deeper? Explore the resources below
Frequently asked questions
Have questions about exhaust gas recirculation (EGR) and its impact on carbon capture, emissions, and plant efficiency? Explore our FAQ to learn the basics, understand the benefits, and discover how EGR can be applied to new and existing power plants.
EGR is the process of redirecting a portion of gas turbine exhaust back to the turbine inlet for re-combustion.
Redirecting exhaust reduces flow to the stack proportionally. For example, at 40% EGR, 40% of exhaust flow is redirected back to the turbine inlet, reducing flow to the stack, and base load emissions of NOx, CO, and particulate matter (PM), by approximately 40%.
EGR reduces the volume of exhaust sent to the carbon capture plant, allowing for smaller components, a reduced footprint, lower costs, and reduced steam usage.
EGR also increases CO2 concentration in the exhaust, creating a stronger driving force for capture. This improves capture efficiency, further reducing plant size and steam usage. Additionally, by lowering oxygen concentration in the exhaust, EGR reduces oxidation driven degradation of the amines used to capture carbon.
Net plant output increases with EGR, primarily due to reduced steam usage in the carbon capture process.
Yes, EGR can be installed in both new and existing combined cycle power plants. It's currently commercially available for the 7HA.03 and 9HA.02 gas turbines, with project specific offerings available for select variants.
EGR lowers CapEx by reducing the size of the carbon capture plant, and lowers OpEx by reducing amine degradation rates and steam usage.
GE Vernova also offers steam integration, which extracts steam for the carbon capture plant directly from the combined cycle steam turbine. This reduces or eliminates the need for an auxiliary boiler, improving site fuel consumption, lowering CapEx and plant size, and reducing site CO2 emissions.
Exhaust Gas Recirculation is designed to work alongside carbon capture to support lower-emission power generation, particularly during part-load operation. EGR increases the CO2 concentration in the exhaust stream, aiming to reduce the energy required to separate CO2 from the solvent and improve overall capture performance.
EGR also aims to reduce reliance on Inlet Bleed Heat (IBH), which is traditionally used to support emissions control and combustion stability. Because IBH diverts compressed air away from the turbine, reducing its use could allow more of that air to go toward power generation. As a result, EGR has the potential to improve both carbon capture efficiency and part-load performance, helping plants lower emissions while working to maintain operational performance.
Contact us