GE Vernova’s rotor management service centers
With GE Vernova’s Center of Excellence approach for repair services, we focus our repair capabilities to achieve consistent, high-quality results.
With a global network of service centers dedicated to rotor life management services and repairs, GE Vernova is continuously investing in the latest tooling and technologies to keep our customers’ rotors running reliably for years to come. Our repair shops are also dedicated to sustainable operations through their support of GE Vernova’s Carbon Neutral Operations 2030 and Net Zero 2050 ambition and metal chip recycling programs with our suppliers, with more than 50% CO2 reduction over the rotor lifecycle when performing an RLE versus a new rotor.
Located in Greenville, South Carolina (USA), GEVernova’s technology center was originally opened as a gas turbine manufacturing plant in 1968. In 2008 the plant was updated and expanded into the world's largest and most comprehensive full-speed, full-load gas turbine validation test facility.
Rotor frame sizes served: 7E, 7F, 7FA, 7HA, 9FA
Rotor capabilities: Rotor inspection, repairs, and rotor life extension services
Facility size: 1,550,000 square feet
Rotor life extensions performed: More than 50 RLEs completed in the last 5 years
Rotor investment: $5 million invested in 2022 to expand rotor repair capability
In addition to serving as a real-world grid environment where gas turbine fleets can be tested and validated well beyond normal power plant conditions, the center also provides gas turbine assembly, repairs, and parts. Special repairs and processes include rotor repair, combustion repair and hot gas path repair.
In 2022, GE Vernova made investments to expand the facility to improve cycle time and quality, as well as increase capacity for building new aeroderivative gas turbines. In 2014, GE Vernova invested $400 million to expand the company’s advanced manufacturing capabilities. In the 5 years before that, GE Vernova invested more than $500m to boost critical manufacturing activities.
The world’s largest gas turbine service center, GEMTEC is located in Dammam, Saudi Arabia, and provides gas turbine components and generator rotors for frame 5, B&E, and 7F/9F.
To date, GEMTEC has serviced more than 70 customers in over 40 countries. Most recently GE Vernova invested about $3 million in GEMTEC to become qualified to perform 7FA rotor life extensions. As a result, GE Vernova was able to perform its first 7FA rotor life management solution in the Middle East.
Rotor frame sizes served: 5, B&E, 7F, 9F
Rotor capabilities: Rotor inspection, repairs, and rotor life extension services
Facility size: 12,000 square meters
Rotor life extensions performed: More than 15 RLEs completed in the last 4 years
Rotor investment: $3 million
The GEMTEC campus includes the GEMTEC Service and Repairs Center for gas turbines, GE Vernova MENA Decarbonization Center of Excellence (COE), a Monitoring & Diagnostics Center for the remote monitoring of power generation assets, as well as GE Vernova Saudi Advanced Turbines (GESAT), a joint investment by Dussur and GE Vernova to manufacture heavy duty gas turbines and components in the Kingdom.
GEMTEC is playing a strong role in helping to achieve the goals outlined under Saudi Vision 2030 by nurturing local talent and suppliers, further diversifying Saudi Arabia’s economic base, promoting exports, and much more.
GE Vernova invested about $3 million in the GEMTEC service center to become qualified to perform 7FA rotor life extensions. GE Vernova employed a seed rotor approach, where a refurbished rotor from GE Vernova’s inventory that has been inspected and updated with the latest technology to maintain safe long-term operation is sent to the customer and the rotor it replaces it sent to GE Vernova’s service center to be refurbished. This approach allows for a series of rotor life extensions and creates the flexibility of an economical solution while eliminating outage risk.
GE Vernova’s investment in GEMTEC increases the overall capacity worldwide of the 7F rotor network and enables rotor life extensions and refurbished rotor work to be done in the Middle East. The investment included purchase of specialty inspection tooling, an ultrasonic testing tank and a balancing machine. GEMTEC is equipped with the same state of the art rotor balance, stacking, and machining equipment as our other global rotor repair centers, providing us with additional capacity to meet global customer needs.
In addition, this investment is helping GE Vernova become closer to our customers by providing 7F rotor repair work in the region—providing customers with reduced lead time (at least 3 months faster than shipping the equipment to other parts of the world) and greater savings.
One of the largest gas turbine service centers
See how GE Vernova's Dammam service center is helping power Saudi Arabia.
Located in Jurong, Singapore, GEVSS is the largest F-class turbine blade repair service center in the world. It’s the first HA-class repair development center outside the U.S., allowing GE Vernova to better serve customers in Asia and other countries around the world.
Recently GE Vernova invested more than $4 million to build up the center’s capability to handle 9F rotor life extensions (RLE) and completed the first 9F rotor life extensions (RLE) at the GEVSS.
Rotor frame sizes served: B&E, 6F, 7F, 9F
Rotor capabilities: Rotor inspection, repairs, and rotor life extension services
Facility size: 545,000 square meters
Rotor life extensions performed: More than 35 RLEs completed in last 5 years
Rotor investment: $4 million to perform F-class RLEs, and a recently approved project to expand HA capability (additional $18-20 million).
One of GE Vernova’s four heavy duty rotor service centers globally, the GEVSS is the largest and only aeroderivative repair service center with combustor DVM coating.
GE Vernova responded to a customer request to perform rotor life extensions with a $4 million investment to add inspection tooling and machines, the installation of the new equipment, and training the machine vendors.
Rotor life extension for F-class rotors is a process GE Vernova has created over many years of experience with design analytics, shop inspections and operating data. Now, with the additional investment, GEVSS can perform RLEs on 7F and 9F RLEs—and the additional capacity has increased the center’s capability by at least 35%.
In addition, this investment is helping GE Vernova become closer to our customers by providing 7F rotor repair work in country—providing customers with reduced lead time (at least 3 months faster than shipping the equipment to other parts of the world) and greater savings.
Take the virtual tour
GE Vernova has 2 industrial centers in France: Gas Turbine and Rotor assembly in Belfort and Rotor and Hot Gas Path in Bourogne.
The Bourogne site manufactures and repairs the critical components of Gas turbines, notably rotors parts, to be assembled by the Belfort location and supplies the turbine blades and combustion parts.
The Belfort site assembles and repairs high-power, high-efficiency 50 Hz gas turbines, including 6B, 6F, 9E, GT13, 9F and 9HA turbines.
Rotor frame sizes served: 6B, 9E, 6FA, 9HA
Rotor capabilities: Rotor inspection, repairs, and rotor life extension services
Facility size: 12,000 square meters
Rotor life extensions performed: 6 RLEs performed over the last 5 years, including the first ever RLE on a 6FA rotor
Rotor investment: $21 million over the last 5 years
A third center is dedicated to the management of customer projects worldwide and on-going research and development for gas turbine technologies.
In addition to serving as a real-world grid environment where gas turbine fleets can be tested and validated well beyond normal power plant conditions, the center also provides gas turbine assembly, repairs, and parts. Special repairs and processes include rotor repair, combustion repair and hot gas path repair.
In 2022, GE Vernova made investments to expand the facility to improve safety, quality and cycle time, as well as expanding the company’s advanced manufacturing capabilities. In the last 5 years, GE Vernova invested 21 million to boost critical manufacturing activities.
Customer stories
Contact us