Prefer to listen?

Stream our audio version

00:00:00 / 00:00:00

~40% of reported F-class reliability issues could have been prevented with upgraded instrumentation and valves.

Do you have questions about reliability challenges seen by F-class gas turbines, such as instrumentation failures, valve malfunctions, or false flame signals? These challenges may cause unplanned outages and costly repairs. Explore our FAQ for answers to commonly asked reliability questions and see how proven upgrades and engineering solutions can help keep your plant running smoothly. Have a question we haven’t covered? Contact our experts for personalized support.

Trips are often linked to four main challenges: flame scanner cooling water leakage, false high exhaust spreads, compressor bleed valve sticking, and false loss of flame. These issues can result in failed starts, trips, forced outages, and extended downtime.

  • Flame scanner cooling water leakage: Increases the risk of turbine rubs due to potential tubing cracks or disconnections, which can lead to compressor rubbing, irreparable damage, and extended downtime.
  • High exhaust spread: Uneven or excessive temperature variation across the turbine exhaust, which can be caused by inaccurate thermocouple readings or premature sensor issues.
  • Compressor bleed valve issues: Occurs when a valve that extracts air from the gas turbine compressor during key operating points in startup or shutdown gets stuck open or closed and does not respond to commands. This issue can be caused by a corroded internal part.
  • Loss of flame: An indication of sudden loss or instability of the combustion flame in the combustor. A malfunctioning flame scanner may cause false loss of flame.

GE Vernova offers several upgrades, including:

  • Non-optical flame detectors (NOFD): A software update for F-class turbines with Mark* VIe controls can help improve the safe operation of your F-class gas turbine and reduce the risk of unplanned outages due to failed flame scanners and leaking water-cooling circuits.
  • Fiber-optic dry flame detectors: Are drop-in replacement flame detectors with fiber optic sensors and remote electronics placement. Can withstand heat and vibration, reducing false trips and improving combustion monitoring for F-class turbines.
  • Robust exhaust thermocouples: Upgraded exhaust thermocouples sensors developed to reduce vibration, tip fretting, and cable failures. Help to improve the accuracy of exhaust temperature readings and help prevent false high exhaust spreads.
  • Stainless steel compressor bleed valves: Stainless steel components replace corrosion-prone valves on 7F or 9F gas turbines' critical cooling and sealing air system. This upgrade helps reduce the risk of valves sticking during startup or shutdown, thereby improving turbine availability and ensuring smoother operation.

GE Vernova offers a wide range of reliability upgrades. Explore our full portfolio and connect with an expert to find the right solution for your plant.

 

Upgrading to non-optical flame detectors (NOFD) or fiber-optic dry flame detectors eliminates the need for water-cooled scanners, removing the risk of casing damage from leaks while providing reliable flame detection.

Start-reliability solutions are critical for plants operating in peaking or daily cycling modes, and for those transitioning to these profiles. GE Vernova offers a comprehensive suite of start reliability upgrades, including OpFlex controls, operability enhancements, and instrumentation and hardware improvements.

Key examples of these solutions are:

  • OpFlex* Start Agility portfolio, with solutions including Start Assurance, can help improve both simple cycle and combined-cycle start reliability. Fast Start, Purge Credit, and Start-up NOx are other start-related solutions in the portfolio.
  • OpFlex variable peak solution enhances control and operability by increasing the firing temperature to a specified level based on the gas turbine’s hardware and combustion system configuration.
  • Instrumentation upgrades such as advanced compressor bleed valves, flame scanners, and gas valves.
  • Flange-to-flange upgrade replaces the existing turbine from inlet to exhaust.

The recommended upgrades depend on each unit’s condition and operating profile. Each plant has site-specific needs. Contact us or your GE Vernova account manager to learn which upgrades are right for your plant.

For seasonal or intermittent operations, we recommend following the GEK28156Q (available in the GE Vernova Customer Portal) procedure, which is included in the plant’s Operation and Maintenance documentation. This document outlines protection and preservation measures for gas turbines and their associated equipment under various conditions, including:

  • Short-term storage: For periods up to one year, beginning when the equipment ships from the factory to storage.
  • Long-term storage: For storage periods exceeding one year.
  • Pre-commissioning and installation: When the unit has arrived on-site but is still in the installation phase.
  • Post-commissioning: When the unit is commercially operational but remains offline for extended periods (e.g., two weeks or more).

By following the GEK28156Q guidelines, users can reduce the risk of reliability challenges when units cycle between operational and preservation states. Contact us or your GE Vernova account manager for more details.

GE Vernova control systems use redundancy and diagnostics, including Triplex Metrics controllers, dual networks, and redundant sensors. This approach helps reduce unnecessary trips and helps protect the unit without relying on a single point of failure.

Users should review all published TILs as they become available, with priority given to those related to safety, compliance, and alert notifications. These carry the highest criticality and should be acted upon first.

Are you unsure if you have any unread TILs? Visit the customer portal to see any unread TILS or contact your account manager.

Need to register for the customer portal? Register today!

GE Vernova is constantly seeking opportunities to enhance and improve our reliability upgrades. We apply learnings and technologies from H-class turbines (9HA and 7HA gas turbines) and utilize F-class fleet data from our engineering teams and customer support cases to develop upgrades that can help improve the reliability and efficiency of the overall F-class fleet.

Houssem-zoghmar_sketched.jpg

"Our upgrades focus on aiming to solve the reliability issues that matter most to operators, helping plants run more safely, efficiently, and with less unplanned downtime.”
 

Houssem Zoghmar, Service Engineering Leader, GE Vernova

Webinar

91M+ operating hours of insight: F-class reliability solutions

Sep 4, 2025 | 3pm MYT, 11am Berlin, 11am NYC

Join our webinar to learn how we can help you reduce trips and failed starts with proven solutions. With over 1.6 million starts across 1,350+ F-class gas turbines, GE Vernova has gained deep insight into reliability challenges.

Mohamed Sayed

Customer Application Engineering, GE Vernova

Noora AlAmiri

Lead Upgrade Sales Manager for Gulf, GE Vernova

Houssem Zoghmar

Service Engineering Leader, GE Vernova

Save time and money with F-class reliability upgrades

We’ve drawn on millions of hours of fleet data and created a solution to keep you running and preserve revenue. Discover the right upgrade for your gas turbine today.

Contact us

Talk to an expert about the best reliability upgrades for your units

*Trademark of GE Vernova and/or its affiliates.